AXIS#.VL.ACCFILTERED

Description

AXIS#.VL.ACCFILTERED returns the filtered acceleration.

Versions

Action Version Notes
Implemented 02-04-01-000

 

General Information

Type

Read Only

Description Depends on AXIS#.UNIT.ACCROTARY
Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.ACCFILTERED

5011h

2ah

Signed32

-

1000:1

Read only

No

AXIS2.VL.ACCFILTERED

5111h

2ah

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6041

1

6041 (0x1799)

AXIS1.VL.ACCFILTERED

Signed32

Read Only

Yes

71577

2

6041 (0x1799)

AXIS2.VL.ACCFILTERED

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.ACCFILTERED

6041

Float

Read Only

Acceleration

Related Topics

Velocity Loop